Determines the number of bytes offset from the current stream position to the beginning of the array.
int pcount() const;
The function pcount() is used to determine the offset of the array. This may not equal to the number of characters inserted due to possible positioning operations.
Returns an int_type that is the length of the array.