To retrieve a pointer to the stream buffer.
basic_stringbuf<charT, traits>* rdbuf() const;
To manipulate a stream for random access or synchronization it is necessary to retrieve a pointer to the streams buffer. The function rdbuf() allows you to retrieve this pointer.
A pointer to an object of type basic_stringbuf sb is returned by the rdbuf function.
Template class basic_istringstream
#include <iostream> #include <iostream> #include <sstream> std::string buf = "CodeWarrior - \"Software at Work\""; char words[50]; int main() { using namespace std; stringstream ist(buf, ios::in); istream in(ist.rdbuf()); in.seekg(25); in.get(words,50); cout << words; return 0; }
Result
"Software at Work"