Remarks
Manipulators are used in the stream to alter the formatting of the stream.
A reference to an object of type
ios_base is returned to the stream. (The
this pointer.)
Prototype of ios_base manipulators
Manipulator
Definition
ios_base&
boolalpha(ios_base&)
insert and extract bool type in alphabetic format
ios_base&
noboolalpha (ios_base&)
unsets insert and extract bool type in alphabetic format
ios_base&
showbase(ios_base& b)
set the number base to parameter b
ios_base&
noshowbase (ios_base&)
remove show base
ios_base&
showpoint(ios_base&)
show decimal point
ios_base&
noshowpoint(ios_base&)
do not show decimal point
ios_base&
showpos(ios_base&)
show the positive sign
ios_base&
noshowpos(ios_base&)
do not show positive sign
ios_base&
skipws(ios_base&)
input only skip white spaces
ios_base&
noskipws(ios_base&)
input only no skip white spaces
ios_base&
uppercase(ios_base&)
show scientific in uppercase
ios_base&
nouppercase (ios_base&)
do not show scientific in uppercase
ios_base& unitbuf (ios_base::unitbuf)
set the unitbuf flag
ios_base&
nounitbuf (ios_base::unitbuf)
unset the unitbuf flag