Header iosfwd

The header <iosfwd> is used for forward declarations of template classes.

The template class basic_ios<charT, traits> serves as a base class for class basic_istream and basic_ostream.

The class ios is an instantiation of basic_ios specialized by the type char.

The class wios is an instantiation of basic_ios specialized by the type wchar_t.