Type SZ_T

A type that represents one of the signed basic integral types. It is used to represent the number of characters transferred in an input/output operation or the size of the input/output buffers.