The function set_union is used to process the sorted union of two ranges.
template<class InputIterator1, class InputIterator2, class OutputIterator> OutputIterator set_union (InputIterator1 first1, InputIterator1 last1, InputIterator2 first2, InputIterator2 last2, OutputIterator result); template<class InputIterator1, class InputIterator2, class OutputIterator, class Compare> OutputIterator set_union (InputIterator1 first1, InputIterator1 last1, InputIterator2 first2, InputIterator2 last2, OutputIterator result, Compare comp);
The end of the constructed range is returned.