generate_n

The function generate_n is used to replace a number of elements with the result of an operation.

  template<class OutputIterator, class Size, class Generator>
  void generate_n
  (OutputIterator first, Size n, Generator gen);
  
Remarks

There is no return value.