grouping

The grouping string specifies the number of digits to group, going from right to left. For example, the grouping: 321 means that the number 12345789 would be printed as in:

  1,2,3,4,56,789

  

The above grouping string can be specified as:

  grouping = 321

  

A grouping string of "0" or "" means: do not group.