This chapter is a reference guide to the ANSI/ISO String class that describes components for manipulating sequences of characters, where characters may be of type char, wchar_t, or of a type defined in a C++ program.
This chapter is constructed in the following sub sections and uses the ISO (International Organization for Standardization) C++ Standard as a guide: