Used when a function-like macro is defined.
EWL_C/src/alloc.c Line: 14 EWL_C/src/alloc.c Line: 63 EWL_C/src/alloc.c Line: 1973 EWL_C/src/alloc.c Line: 2493 EWL_C/src/alloc.c Line: 2559 EWL_C/src/bsearch.c Line: 24 EWL_C/src/buffer_io.c Line: 121 EWL_C/src/coldfire/fenv_cf.c Line: 31 EWL_C/src/mem_funcs.c Line: 72 EWL_C/src/qsort.c Line: 64 EWL_C/src/scanformat.c Line: 140 EWL_C/src/string.c Line: 816 EWL_C/src/strtold.c Line: 232 EWL_C/src/strtoul.c Line: 98 EWL_C/src/sun_math/Double_precision/k_standard.c Line: 19 EWL_C/src/wcstold.c Line: 202 EWL_C/src/wcstoul.c Line: 107