Used when the symbol usage is consistent with its initialization.
EWL_C/src/sun_math/Double_precision/e_exp.c Line: 182 EWL_C/src/sun_math/Double_precision/k_rem_pio2.c Line: 191 EWL_C/src/sun_math/Double_precision/k_rem_pio2.c Line: 204 EWL_C/src/sun_math/Double_precision/k_rem_pio2.c Line: 223 EWL_C/src/sun_math/Double_precision/k_rem_pio2.c Line: 322 EWL_C/src/sun_math/Single_precision/k_rem_pio2f.c Line: 96 EWL_C/src/sun_math/Single_precision/k_rem_pio2f.c Line:108 EWL_C/src/sun_math/Single_precision/k_rem_pio2f.c Line:123 EWL_C/src/sun_math/Single_precision/k_rem_pio2f.c Line:220