The CodeWarrior Development Studio for Microcontrollers V10.x MISRA-C:2004 Compliance Exceptions for the HC(S)08, RS08, COldFire, Kinetis and Power Architecture Libraries manual covers the MISRA-C:2004 compliance exceptions for the HC(S)08, RS08, ColdFire, Kinetis and Power Architecture libraries.
This document contains following chapters:
Chapter 2 - HC(S)08 contains the list of MISRA-C:2004 exceptions for HC(S)08
Chapter 3 - RS08 contains the lists of MISRA-C:2004 exceptions for RS08
Chapter 4 - ColdFire contains the lists of MISRA-C:2004 exceptions for ColdFire
Chapter 5 - Kinetis contains the lists of MISRA-C:2004 exceptions for Kinetis
Chapter 6 - Power Architecture contains the lists of MISRA-C:2004 exceptions for Power Architecture
For a particular target, either HC(S)08, RS08, ColdFire, Kinetis or Power Architecture, the exceptions to MISRA rules are grouped into general exceptions, which apply across all the library projects, and per-project exceptions, which are the exceptions associated with a certain library project. The latter are listed in the order in which they would be identified if the library projects were checked against MISRA rule violation using the PC-Lint tool - one by one, in the same order as the corresponding chapter sections (for example: C Startup, C Startup Tiny, C Startup HCS08 and so on, for HC(S)08).