Adding properties

You can set one of the properties of the component: even or odd parity.

Right-click on the Properties in the Component editor and select Add Property option from the context menu to open the Properties editor.
Figure 1. Properties editor



The ItemLevel item represents the user level at which the item is accessible in the Processor Expert interface. All users can see it. Some properties are for advanced or expert users only.

You can provide text in Hint if you wish. This is a context help that pops up over the property when you hover the cursor.