A macro command must start at the beginning of the line (% as the first non-space character on the line); this line may contain only this command. The remainder of the line is a comment. For a macro command, a comment up to the end of line can also be used in the following format: %--.
A list of macro commands by type follows under these topics: