This document describes the macro-processor embedded in PE serving namely for component code generation based on the component driver. It defines the syntax and semantics of the macro-processor, as well as the symbols predefined including their importance. In addition, TST and CHG script files are described herein. This manual is composed of the following chapters:
| Chapter Title | Description |
|---|---|
| Introduction | Provides the introduction of the manual. |
| Terms and Definitions | Describes the terms and definitions used in the manual. |
| Processor Expert Macro-language Description | Describes the symbols and commands for Processor Expert Macro-language. |
| TST Script for Component Testing | Describes the TST script files for component testing. |
| Component Scripts | Describes the setting control script for CHG script files |
| TS2 Script for Component Interdependence Testing | Describes the TS2 script file for component interdependence testing. |
| CDB | Describes the CDB files. |
| External Libraries | Describes the external libraries API. |