syspath_once

Controls how include files are treated.

Syntax
  #pragma syspath_once on | off | reset  
Remarks

If you enable this pragma, files called in #include <> and #include "" directives are treated as distinct, even if they refer to the same file.

This pragma does not correspond to any panel setting in the Language panel. To check this setting, use __option (syspath_once), described in Checking Pragma Settings. By default, this setting is enabled. For example, the same include file could reside in two distinct directories.

C Standard Library and Runtime Library (CW libraries) functions require the AGU (Address Generation Unit) to be in linear addressing mode, that is, the M01 registers are set to -1. If a function is interrupted and was using modulo address arithmetic, any calls to CW libraries from the ISR do not work unless the M01 is set to -1 in the ISR. Also, the M01 register would need to be restored before exiting the ISR so that the interrupted function can resume as before, with the same modulo address arithmetic mode settings.