Controls the use of common subexpression optimization.
#pragma opt_common_subs on | off | reset
If you enable this pragma, the compiler replaces similar redundant expressions with a single expression. For example, if two statements in a function both use the expression
a * b * c + 10
the compiler generates object code that computes the expression only once and applies the resulting value to both statements.
The compiler applies this optimization to its own internal representation of the object code it produces.
This pragma does not correspond to any panel setting in the Language panel. To check this setting, use __option (opt_common_subs), described in Checking Pragma Settings. By default, this pragma is disabled.