Adds an item to the Function pop-up menu in the IDE editor.
#pragma mark itemName
This pragma adds itemName to the source file's Function pop-up menu. If you open the file in the CodeWarrior Editor and select the item from the Function pop-up menu, the editor brings you to the pragma. Note that if the pragma is inside a function definition, the item does not appear in the Function pop-up menu.
If itemName begins with "-", a menu separator appears in the IDE's Function pop-up menu:
#pragma mark -
This pragma does not correspond to any setting in the Language panel. By default, this pragma is disabled.