__MWERKS__

Defined with the version of the CodeWarrior compiler.

CodeWarrior compilers issued after 1995 define this macro with the compiler's version. For example, if the compiler version is 3.2, the value of __MWERKS__ is 0x3200.

This macro is defined as 1 if the compiler was issued before the CodeWarrior CW7 that was released in 1995.