Setting the PATH Environment Variable

The PATH variable should include the paths for the 56800/E tools as shown in the following listing.

Listing: Example of PATH Settings


%CWFolder%\MCU\DSP56800x_EABI_Tools\command_line_tools

In order for FlexLM to work properly, you can simply copy the following file into the directory from which you will be using the command line tools:

  

..\CW MCU v10.x\MCU\license.dat

Alternately, you can define the variable LM_LICENSE_FILE as:

 

 %CWFolder%\MCU\license.dat 

This variable points to license information. It may point to alternate versions of this file, as needed.