Configuring Command-Line Tools

To use the command-line tools, several environment variables must be changed or defined.

If you are using CodeWarrior command-line tools with Microsoft Windows, environment variables may be assigned in Environment variables under System Properties of control panel.

The CodeWarrior command-line tools refer to environment variables for configuration information: