Controls whether the compiler uses additional environment variables to provide default settings.
-defaults -[no]defaults
This command is global. To enable the command-line compiler to use the same set of default settings as the CodeWarrior IDE, use -defaults. For example, in the IDE, all access paths and libraries are explicit. defaults is the default setting.
Use -nodefaults to disable the use of additional environment variables.