Use this panel to specify the command, options, and expert settings for DSC Disassembler.
The following table lists and describes the disassembler options for DSC.
| Option | Description |
|---|---|
| Command | Shows the location of the disassembler executable file. Default value is ""${DSC_ToolsDir}/mwld56800e". You can specify additional command line options for the disassembler; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the disassembler will be called with. |
| Expert settings Command line pattern |
Shows the expert settings command line parameters; default is ${COMMAND} -dis ${FLAGS} ${INPUTS} |