The compiler uses registers A,B, R1, R2, R3, R4, Y0, and Y1 to pass parameter values to functions. Upon a function call, the compiler scans the parameter list from left to right, using registers for these values:
The compiler passes the remaining parameter values on the stack. The system increments the stack by the total amount of space required for memory parameters. This incrementing must be an even number of words, as the stack pointer (SP) must be continuously long-aligned. The system moves parameter values to the stack from left to right, beginning with the stack location closest to the SP. Because a long parameter must begin at an even address, the compiler introduces one-word gaps before long parameter values, as appropriate.