Deadstripping and Link Order

The M56800E Linker deadstrips unused code and data only from files compiled by the CodeWarrior C compiler. The linker never deadstrips assembler relocatable files or C object files built by other compilers.

Libraries built with the CodeWarrior C compiler contribute only the used objects to the linked program. If a library has assembly files or files built with other C compilers, the only files that contribute to the linked program are those that have at least one referenced object. If you enable deadstripping, the linker completely ignores files without any referenced objects.

The Link Order page of the project window specifies the order (top to bottom) in which the DSP56800E linker processes C source files, assembly source files, and archive (.a and .lib) files. If both a source-code file and a library file define a symbol, the linker uses the definition of the file that appears first, in the link order. To change the link order, drag the appropriate filename to a different place, in this page’s list.