To transfer the run control connection from the dummy project into the original one:
- Select Window > Show View > Remote Systems to open the Remote
Systems view.
- If the original and dummy projects are the only open projects in the workspace, the
Remote System view lists the connections for these two projects only. However, there might
be some additional connections on the list, which are usually stored directly in the
workspace settings. For example Flash Programmer connections.
Figure 1. Remote systems view
Note: The connections are represented by the

icon:
- Select the connection from dummy project
(My_CW_project_dummy_FLASH_OSJTAG) and apply it to the debug configuration created in previous
step (My_CW_project_FLASH_OSJTAG).
- Right-click on connection to transfer and from the shortcut menu select Apply To
Project > <Name of the original project> > New debug
configuration.
Figure 2. Transfer connection
- Close the dummy project.