The new debug configuration of the original project will need some final edit\adjustments. It
is necessary to ensure that the project uses the right connection transferred from the dummy
project. To make adjustements to the new debug configurations:
- Open the debug configurations dialog.
- Select the new debug configuration created, refer Clone/Duplicate debug configuration.
In this example the new debug configuration is My_CW_project_FLASH_OSJTAG .
The
new connection (My_CW_project_dummy_FLASH_OSJTAG) will appear in the list of
available connections.
- Select the new connection.
Figure 1. Edit connection
- Rename the dummy connection and the target name
(My_CW_project_dummy_FLASH_OSJTAG) since it has inherited the name of the dummy
project in its name.
- To rename the dummy connection and the target name, click the Edit
button.
- Change the connection Name field in the Hardware or Simulator
Connection dialog. For example, My_CW_project_FLASH_OSJTAG.
- Change the target Name field in the Hardware or Simulator
Target dialog.
Figure 2. Select the dummy connection and the target
Figure 3. Rename the dummy connection and the target
- Delete the dummy project.
The connection/run control interface is now the integral part of
the original project.