Create a dummy project

Create a new bareboard project. Ensure that the new project is located in the same workspace as the original project. Provide a different name to the dummy project, for example: My_CW_dummy_project”.
Note: Multiple projects of the same name cannot exist in the same workspace.
Note: The connection configuration/target names inherit the project name. The project will be renamed later to match with the original project name.
This new project must select exactly the same microcontroller derivative as the original project (MPC5602P). The new project should also include the connection(s) you would like add into the original project. Both projects – original and dummy need to be opened in the workspace to be able transfer connection configuration form each other.
Figure 1. Select a connection

Select a connection