The syntax for an attribute specification is
__attribute__(( list-of-attributes ))
where list-of-attributes is a comma-separated list of zero or more attributes to associate with the object. Place an attribute specification at the end of the delcaration and definition of a function, function parameter, or variable. Example of an attribute specification shows an example.
int f(int x __attribute__((unused))) __attribute__((never_inline));
int f(int x __attribute__((unused))) __attribute__((never_inline))
{
return 20;
}