Pragma Scope

The scope of a pragma setting is limited to a compilation unit (a source code file and the files that it includes).

At the beginning of compilation unit, the compiler uses its default settings. The compiler then uses the settings specified by the CodeWarrior IDE's build target or in command-line options.

The compiler uses the setting in a pragma beginning at the pragma's location in the compilation unit. The compilers continues using this setting:

Related information
Checking Pragma Settings
Saving and Restoring Pragma Settings
Determining Which Settings Are Saved and Restored
Invalid Pragmas