auto_inline

Controls which functions to inline.

Syntax
#pragma auto_inline on | off | reset
  
Remarks

If you enable this pragma, the compiler automatically chooses functions to inline for you, in addition to functions declared with the inline keyword.

Note that if you enable either the Do not Inline setting or the dont_inline pragma, the compiler ignores the setting of the auto_inline pragma and does not inline any functions.

This pragma corresponds to the Auto-Inline setting in the CodeWarrior IDE's Properties > C/C++ Build > Settings > Tool Settings > PowerPC Compiler > C/C++ Language settings panel. By default, this pragma is disabled.

Related information
access_errors
always_inline
arg_dep_lookup
ARM_conform
ARM_scoping
array_new_delete
bool
cplusplus
cpp1x
cpp_extensions
debuginline
def_inherited
defer_codegen
defer_defarg_parsing
direct_destruction
direct_to_som
dont_inline
ecplusplus
exceptions
inline_bottom_up
inline_bottom_up_once
inline_depth
inline_max_auto_size
inline_max_size
inline_max_total_size
internal
iso_templates
new_mangler
no_conststringconv
no_static_dtors
nosyminline
old_friend_lookup
old_pods
old_vtable
opt_classresults
parse_func_templ
parse_mfunc_templ
RTTI
suppress_init_code
template_depth
thread_safe_init
warn_hidevirtual
warn_no_explicit_virtual
warn_no_typename
warn_notinlined
warn_structclass
wchar_type