parse_mfunc_templ

Controls whether or not to use the new parser supported by the CodeWarrior 2.5 C++ compiler for member function bodies.

Syntax
#pragma parse_mfunc_templ on | off | reset
  
Remarks

If you enable this pragma, member function bodies within your C++ source code is compiled using the newest version of the parser, which is stricter than earlier versions.

This pragma does not correspond to any panel setting. By default, this pragma is disabled.

Related information
access_errors
always_inline
arg_dep_lookup
ARM_conform
ARM_scoping
array_new_delete
auto_inline
bool
cplusplus
cpp1x
cpp_extensions
debuginline
def_inherited
defer_codegen
defer_defarg_parsing
direct_destruction
direct_to_som
dont_inline
ecplusplus
exceptions
inline_bottom_up
inline_bottom_up_once
inline_depth
inline_max_auto_size
inline_max_size
inline_max_total_size
internal
iso_templates
new_mangler
no_conststringconv
no_static_dtors
nosyminline
old_friend_lookup
old_pods
old_vtable
opt_classresults
parse_func_templ
RTTI
suppress_init_code
template_depth
thread_safe_init
warn_hidevirtual
warn_no_explicit_virtual
warn_no_typename
warn_notinlined
warn_structclass
wchar_type