Controls which warning numbers are displayed during compiling.
#pragma warning on | off | reset ( num [, ...])
This alternate syntax is allowed but ignored (message numbers do not match):
#pragma warning ( warning_type : warning_num_list [, warning_type : warning_num_list , ...])
num
The number of the warning message to show or suppress.
warning_type
Specifies one of the following settings:
warning_num_list
The warning_num_list is a list of warning numbers separated by spaces.
Use the pragma showmessagenumber to display warning messages with their warning numbers.
This pragma only applies to CodeWarrior front-end warnings. Using the pragma for the Power Architecture back-end warnings returns invalid message number warning.
The CodeWarrior compiler allows, but ignores, the alternative syntax for compatibility with Microsoft® compilers.
This pragma does not correspond to any panel setting. By default, this pragma is on .