Controls the usage of Complete Program IPA mode by the compiler.
#pragma ipa_not_complete on | off | reset
In Complete Program IPA mode, the compiler assumes that the IPA graph is complete and that there are no external entry points other than main() , static initialization or force export functions. The compiler will not use this mode if the
The Complete Program IPA mode is not used by the compiler if:
Any extern object that is not main() , static initialization code or force export and not directly or indirectly used, will be deadstipped by the compiler and will not appear in the object and/or executable files. By default, this setting is off .