strictheaderchecking

Controls how strict the compiler checks headers for standard C library functions.

Syntax
#pragma strictheaderchecking on | off | reset
  
Remarks

The 3.2 version compiler recognizes standard C library functions. If the correct prototype is used, and, in C++, if the function appears in the " std " or root namespace, the compiler recognizes the function, and is able to optimize calls to it based on its documented effects.

When this #pragma is on (default), in addition to having the correct prototype, the declaration must also appear in the proper standard header file (and not in a user header or source file).

This pragma does not correspond to any panel setting. By default, this pragma is on.

Related information
global_optimizer
ipa
ipa_inline_max_auto_size
ipa_not_complete
load_store_elimination
opt_common_subs
opt_dead_assignments
opt_dead_code
opt_lifetimes
opt_loop_invariants
opt_propagation
opt_strength_reduction
opt_strength_reduction_strict
opt_unroll_loops
opt_vectorize_loops
optimization_level
optimize_for_size
optimizewithasm
pack