Live Range Splitting

Live range splitting attempts to reduce the number of variables used in a function. This optimization reduces a function's runtime stack size, requiring fewer instructions to invoke the function. This optimization potentially improves execution speed.

Controlling live range splitting explains how to control the optimization for live range splitting.

Table 1. Controlling live range splitting
Turn control this option from here... use this setting
CodeWarrior IDE Choose an Optimization Level value (3,4) from the Properties > C/C++ Build > Settings > Tool Settings > PowerPC Compiler > Optimization panel.
source code There is no pragma to control this optimization.
command line -opt level=3 , -opt level=4

For example, in Before live range splitting three variables, a , b , and c , are defined. Although each variable is eventually used, each of their uses is exclusive to the others. In other words, a is not referred to in the same expressions as b or c , b is not referred to with a or c , and c is not used with a or b .

In After live range splitting , the compiler has replaced a , b , and c , with a single variable. This optimization reduces the number of registers that the object code uses to store variables, allowing more variables to be stored in registers instead of slower memory. This optimization also reduces a function's stack memory.

Figure 1. Before live range splitting
void func_from(int x, int y)
{
    int a;
    int b;
    int c;

    a = x * y;
    otherfunc(a);

    b = x + y;
    otherfunc(b);

    c = x - y;
    otherfunc(c);
}
Figure 2. After live range splitting
void func_to(int x, int y)
{
    int a_b_or_c;

    a_b_or_c = x * y;
    otherfunc(temp);

    a_b_or_c = x + y;
    otherfunc(temp);

    a_b_or_c = x - y;
    otherfunc(temp);
}