The dead code elimination optimization removes expressions that are not accessible or are not referred to. This optimization reduces size and increases execution speed.
Controlling dead code elimination explains how to control the optimization for dead code elimination.
| Turn control this option from here... | use this setting |
|---|---|
| CodeWarrior IDE | Choose an Optimization Level value (1,2,3,4) from the Properties > C/C++ Build > Settings > Tool Settings > PowerPC Compiler > Optimization panel. |
| source code | #pragma opt_dead_code on | off | reset |
| command line | -opt [no]deadcode |
In Before dead code elimination , the call to func1() will never execute because the if statement that it is associated with will never be true. Consequently, the compiler can safely eliminate the call to func1() , as shown in After dead code elimination .
void func_from(void)
{
if (0)
{
func1();
}
func2();
}
void func_to(void)
{
func2();
}