When the GCC extensions setting is on, the compiler will not issue an error when you declare a static array without specifying the number of elements in the array if you later declare the array completely. Forward declaration of an empty array shows an example.
static int a[]; /* Allowed only when GCC extensions are on. */ /* ... */ static int a[10]; /* Complete declaration. */