The directive SHORTEN_NAMES_FOR_TOR_101 instructs the linker to shorten long template names for the benefit of the WindRiver® Systems Target Server. To use this directive, simply add it to the linker command file on a line by itself.
SHORTEN_NAMES_FOR_TOR_101
WindRiver Systems Tornado Version 1.0.1 (and earlier) does not support long template names as generated for the MSL C++ library. Therefore, the template names must be shortened if you want to use them with these versions of the WindRiver Systems Target Server.