MAX_BIN_GAP

Controls the maximum gap size value between two segments.

MAX_BIN_GAP(nnnnn)

Parameters

nnnnn

Size of the maximum gap allowed between segments.

Remarks

The directive can be placed in the LCF anyway except within the MEMORY and SECTIONS directives.

This directive can only be used if you are generating a single binary file.