Naming Conventions

Power Architecture command line tools lists the names of the CodeWarrior command line tools.

Table 1. Power Architecture command line tools
This tool... does these tasks...
mwasmeppc translates assembly language source code into object code
mwcceppc translates C and C++ source code into object code
mwldeppc links object code into a loadable image file
Related information
Specifying Source File Locations
Licensing Command-Line Options
Diagnostic Command-Line Options
Library and Linking Command-Line Options
Code Generation Command-Line Options
Optimization Command-Line Options