Specifies the end-of-line style to use in an S-record file.
-sreceol keyword
The choices for keyword are:
mac
Use Mac OS®-style end-of-line format.
dos
Use Microsoft® Windows®-style end-of-line format. This is the default choice.
unix
Use a UNIX-style end-of-line format.
This option also generates an S-record file if the -srec option has not already been specified.
This is a linker option.