Sets the loading address of the data.
-dataaddr addr
The addr value is an address, in decimal or hexadecimal format. Hexadecimal values must begin with 0x. The default is the address after the code and large constant sections.
The linker ignores this option if the linker is invoked with the -lcf option.
This is a linker option.