Activating EC++

The table below describes the settings used to control Embedded C++ conformance.

Table 1. Controlling Embedded C++ conformance
To control this option from here... use this setting
CodeWarrior IDE EC++ Compatibility Mode in the C/C++ Language Settings panel
source code #pragma ecplusplus
command line -dialect ec++

To test for EC++ compatibility mode at compile time, use the __embedded_cplusplus predefined symbol.