Specifies inline options. Default settings are smart, noauto.
-inline keyword
The options for keyword are:
off | none
Turns off inlining.
on | smart
Turns on inlining for functions declared with the inline qualifier. This is the default.
auto
Attempts to inline small functions even if they are declared with inline.
noauto
Does not auto-inline. This is the default auto-inline setting.
deferred
Refrains from inlining until a file has been translated. This allows inlining of functions in both directions.
level=n
Inlines functions up to n levels deep. Level 0 is the same as -inline on. For n, enter 1 to 8 levels. This argument is case-sensitive.
all
Turns on aggressive inlining. This option is the same as -inlineon, -inlineauto. This does not turn on the aggressive_inline feature.