Tutorial project for Kinetis microcontrollers

This simple tutorial describes a periodically blinking LED project. The LED is connected to one pin of the CPU and it is controlled by a periodical timer interrupt.

The project is designed to work with PK60N512 CPU and TWR-K60N512 tower board. However, it is not necessary to have this hardware. The project can be created without it.

This simple Processor Expert demo-project uses the following LDD Embedded Components (see Component categories topic for details):

This tutorial contains the following main steps: