Running application
- Build the project using the Project > Build command from the CodeWarrior menu.
- If you have the TWR-K60N512 board, connect it now. Run and debug the application using the Run > Run command from the CodeWarrior menu. When the application starts running, one of the on-board LEDs starts blinking.