This topic explains the options of usage of the complex timers in the high-level components allowing you to benefit from the advanced features of these components. All peripherals from this group are also supported by the Peripheral Initialization Components (for details, see Component categories topic).
The following table shows a list of the timer components and PE devices that can be used in the components as rows. The columns show the state of all devices defined for the timer for conditions determined by rows.
| Component Selected | Selected device(s) | PE devices defined for the timer | |||||
|---|---|---|---|---|---|---|---|
| TIMx | TIMxy | TIMxfree | TIMx_PPG | TIMxPP | TIMxyPPG | ||
| PWM | TIMxy | Blocked | Used 1 channel (2 in buffered mode) Others free | Blocked | Blocked | Blocked | Blocked |
| PPG | TIMxPP TIMxyPPG | Blocked | All channels blocked | Blocked | Used | Used | Used |
| TimerOut | TIMxy | Blocked | Used 1 channel (2 in buffered mode) Others free | Free | Blocked | Blocked | Blocked |
| TimerInt RTIShared TimeDate FreeCntr8 FreeCntr6 FreeCntr32 | TIMxy | Blocked | Used 1 channel Others free | Free | Blocked | Blocked | Blocked |
| TIMxfree | Blocked | All channels free | Used | Blocked | Blocked | Blocked | |
| EventCntr8 EventCntr16 EventCntr32 | TIMx | Used | All channels blocked | Blocked | Blocked | Blocked | Blocked |
| Capture | TIMxy | Blocked | Used 1 channel Others free | Free | Blocked | Blocked | Blocked |
Table legend: