User changes in generated code

It's necessary to say at the beginning of the chapter, that modification of the generated code may be done only at user's own risk. Generated code was thoroughly tested by the skilled developers and the functionality of the modified code cannot be guaranteed. We strongly don't recommend modification of the generated code to the beginners. See more information for generated modules in Code generation topic.

To support user changes in the component modules, Processor Expert supports the following features: