Init method is defined in all Peripheral Initialization Components. Init method contains a complete initialization of the peripheral according to the component's settings.
In the following examples, let's assume a component named "Init1" has been added to the project.
The Init method of the Peripheral Initialization component can be used in two ways: